Bfs Service
You have created a service.
To test this service, you will need to create a client and use it to call the service. You can do this using the svcutil.exe tool from the command line with the following syntax:
svcutil.exe http://aos-core.azurewebsites.net/Bfs.svc/mex
This will generate a configuration file and a code file that contains the client class. Add the two files to your client application and use the generated client class to call the Service. For example:
C#
class Test { static void Main() { BfsClient client = new BfsClient(); // Use the 'client' variable to call operations on the service. // Always close the client. client.Close(); } }
Visual Basic
Class Test Shared Sub Main() Dim client As BfsClient = New BfsClient() ' Use the 'client' variable to call operations on the service. ' Always close the client. client.Close() End Sub End Class