Ticket Service


You have created a service.

To test this service, you will need to create a client and use it to call the service. You can do this using the svcutil.exe tool from the command line with the following syntax:


svcutil.exe http://aos-core.azurewebsites.net/Ticket.svc/mex

This will generate a configuration file and a code file that contains the client class. Add the two files to your client application and use the generated client class to call the Service. For example:

C#


class Test
{
    static void Main()
    {
        TicketClient client = new TicketClient();

        // Use the 'client' variable to call operations on the service.

        // Always close the client.
        client.Close();
    }
}

Visual Basic


Class Test
    Shared Sub Main()
        Dim client As TicketClient = New TicketClient()
        ' Use the 'client' variable to call operations on the service.

        ' Always close the client.
        client.Close()
    End Sub
End Class